Cancel
Showing results for 
Search instead for 
Did you mean: 

CSV import to Process simulate

Creator
Creator

Hello All

 

Can anyone tell me the procedure to import weld points to PS study 

 

I have one excel file and IGES file 

1 REPLY

Re: CSV import to Process simulate

Valued Contributor
Valued Contributor

hello

 

should change the weld spots information into CSV File

 

and the format is as below similar

 

the product which you want to project weld spots should be always in the original frame, can not move it to other frame

 

NAMEXYZ
61158_01_L2290.008-631.31072.373
61158_01_R2290.008631.31072.373
61158_02_L2249.508-631.31068.873
61158_02_R2249.508631.31068.873
61158_03_L2204.508-631.31065.373
61158_03_R2204.508631.31065.373
61158_04_L2163.506-631.31061.468
61158_04_R2163.506631.31061.468
61158_05_L2315.201-656.951074.136
61158_05_R2315.201656.95021074.136
61555_03_L2650.871-103.8221592.633
61555_03_R2650.871103.82171592.633
61555_07_L2665.055-308.9541587.04
61555_07_R2665.055308.95391587.04