Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't import CEE Example project for WKP315S

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter

I have an issue that has wondered me for a while now, but couldn't find an answer yet.
My question is: Where can i import the "CEE Example project" from?
In the activities from the course WKP315S and WKP215S, it says "select the CEE Example project" but no such project was ever imported, and it also has no refference on how to import it in the calssroom setup file.
For example for the WKP115S there is the "Robotic Sim Begin" project and it clearly says in the classroom setup file, under Additional Configuration Requrements: "import the eMS project .XML file from the .\ems_data\sysroot\import export files\Robotics Sim Import to begin042010.xml (once per student)"

There is probably another .xml file which needs to be imported but i can't find it anyhere(it's not in the 'import export files' folder from the ALL_V101_eMS_Data/sysroot).

Can somebody help me with this?

4 REPLIES

Re: Can't import CEE Example project for WKP315S

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Can you please let us know which product you are using and which training guide you are following to complete the mentioned task

Re: Can't import CEE Example project for WKP315S

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter

I'm using Process Simulate 10.1 the training guide is as mentioned WKP315S.

Re: Can't import CEE Example project for WKP315S

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
Thanks, we will try to get you some help.

Re: Can't import CEE Example project for WKP315S

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Go to this folder in the training data: . \sysroot\Imports-Exports and import Event Based Example Project_092512.xml once for each student.

 

This data is used for the WKP215S and WKP315S courses.

 

Yuval