Cancel
Showing results for 
Search instead for 
Did you mean: 

Change 3D graphic of frame

Experimenter
Experimenter

Hello. Does anyone know how to change the 3D graphic of a Frame-object placed inside another Frame? When I select the 'Open in 3D' option for the inserted Frame, it only opens the 3D model within that Frame. Regards

2 REPLIES 2

Re: Change 3D graphic of frame

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Abyss_Above,

For the representation of a frame the graphics in the graphic group default is used.

By default this graphic group is not shown inside the network.

In the View ribbon you have a button to show it. Then just delete the existing graphic and create the graphic you want in the graphic group default.

Just make sure that you want to change it only for the single instance of this frame object, otherwise you should change the graphic in the class object, so that all other instances inherit this graphic.

 

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Change 3D graphic of frame

Experimenter
Experimenter
Thanks again Ralf