05-06-2016 08:18 AM
Hello All,
I have converted NX10 data to .JT , but iam unable to open it in Process Simulate 11.1 ,
It Shows some error .
But when is convert NX9 data to .JT iam able to open it in Process Simulate 11.1 , Is there any option that i can use NX10 and open this .jt data in Process Simulate 11.1
06-30-2016 05:07 PM
I'm not sure if that helps, but worth a try.
There are several versions of JT format. The newer NX you use, the newer JT format it uses by default. A probable reason is that rather old version of PS cannot read the recent JT format.
When you export JT from NX, you can see a path to configuration file (like C:\Siemens\NX10.0\PVTRANS\tessUG.config). This configuration file has much more options than an export dialog.
Try to open it in text editor, search for the line
JtFileFormat = "10"
Replace 10 to 9.5, save configuration and export JT.
06-30-2016 05:16 PM
By the way, there's a hint in Process Simulate. If you try to export JT from a loaded study, you can see a dialog with choice of JT versions.
For example, PS 13 gives the following list:
10.0 (TC Vis 10.1, TX 11.1TR3)
9.5 (TC Vis 8.3, TX 9.1.1)
9.4 (...)
9.1 (...)
8.2 (...)
Watch Replays of Previous Topics