Cancel
Showing results for 
Search instead for 
Did you mean: 

Converter conveyor component side

Experimenter
Experimenter

Hi all,

 

I need a Method to return the side that the MU is waiting for entering in the converter belt.

For the example in the Attached document the method should return 1 : that means there is a MU in the side 1 waiting to enter.

Is there an atrribute that we can use directly?

 

Thanks

Omar

 

 

2 REPLIES

Re: Converter conveyor component side

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Omar,

 

there is a method "getNextEntranceNumber" which returns the number of the side the MU is waiting.

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Converter conveyor component side

Experimenter
Experimenter

thanks Karola

 

Omar