Cancel
Showing results for 
Search instead for 
Did you mean: 

Deinstallation of old Process Simulate Versions

Valued Contributor
Valued Contributor

Hello everybody,
I have an issue here. I am trying to switch the version from 13.0.0 to 13.0.1 via the Version Selector, but receive the error that no oracle client is installed.
I just want to use the standalone version, so I tried to reinstall the 13.0.1 Version, but the setup is not working, claiming that it is not the currently selected version and I should change it in the version selector. Do you have any suggestions?

Thanks in advance.

Kind Regards,

 

Mario