Cancel
Showing results for 
Search instead for 
Did you mean: 

Does Tc MPP works with occurence effectivity?

Valued Contributor
Valued Contributor

@jfacurie 

I'm posting your messaging in our public forum. One of our experts should be able to help you out with this question.

 

Hello,

 

I have a question regarding Collaboration context in TC manufacturing.

 

Does it work with occurence effectivity ?

 

I've seen in your videos that it was possible to configure a BOM along with revision rules, effectivity and variants.

In MPP, can we use revision effectivities AND/OR occurence effectivity to configure a BOM ?

 

Thanks in advance.

 

Best regards

6 REPLIES

Re: Does Tc MPP works with occurrence effectivity?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Yes. We can configure the EBOM with Occ effecticity and it will automatically configure the Process to reflect the changes.

 

Starting TC 9123 you can also see the Occ Effectivity on the consumed part in BOP.

 

When we say effectivity, it means all three are supported. Rev Effectivity, Occ Effectivity and IC effectivity.

 

When you create or save as CC, it will also consider Occ Effectivity (as this is derived by date also).

 

If you any further questions, please let us know.

 

Good Luck!

Re: Does Tc MPP works with occurrence effectivity?

Experimenter
Experimenter

Hello and thanks for your answer.

 

In order to align E-BOM & M-BOM and also compare any changes with acountability checks, do I need the manufacturing module to use MPP, collaboration context and functionalities such as accountability checks ?

 

If yes Is it possible to align and compare BoMs with multi-structure manager for example ?

or your recommendation is to have manufacturing module

 

The thing is I really don't precisely what brings the manufacturing module in term of perspective and functionalities.

 

thanks for your help.

 

 

Re: Does Tc MPP works with occurrence effectivity?

Valued Contributor
Valued Contributor

Accountability check feature is part of MPP application, and you would need the Teamcenter Manufacturing module to access this feature. I don't think accountability check is part of multi structure editor. In multi structure editor you can compare BOMs but that is different from accountability check

Re: Does Tc MPP works with occurrence effectivity?

Experimenter
Experimenter

Hello,

 

Thanks again for your answer.

 

I have another question on the same topic regarding : collaboration context.

 

Again, is it linked to Teamcenter manufacturing or can we create a collaboration context object and use it in Multi structure manager or somewhere else ?

 

Regards

Fabien

Re: Does Tc MPP works with occurrence effectivity?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
The Collaboration Context can be used in multiple perspectives in Teamcenter including MPP and Multi-Structure Manager.

Thanks,

Michael Mood
Solutions Consultant
Siemens PLM Software Inc.
38695 Seven Mile Rd. Ste 300
Livonia, MI 48152
Ph: (734)953-3827
Cell: (248)470-0865

Re: Does Tc MPP works with occurrence effectivity?

Experimenter
Experimenter

Hello,

 

A detail regarding this thread : is all we are saying true for Teamcenter 8.3.3 ?

 

Or just starting at TC9 ?

 

Thanks.