Cancel
Showing results for 
Search instead for 
Did you mean: 

Does tecnomatix plant simulation can be installed on cloud

Creator
Creator

Hi Team,,

 

 

Please let me know does tecnomatix plant simulation can installed on cloud, If yes, please let me know it can be on MS azure or any other cloud platform.

 

 

Thanks

Amar Singh

1 REPLY

Re: Does tecnomatix plant simulation can be installed on cloud

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Amar_Singh,

 

If you have a virtual machine in the cloud which is running at least Windows 7 SP1 Plant Simulation can be installed.

This is offered by Microsoft Azure as well as AWS.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.