Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Elevation views do not show FCAD cylinders correctly - ACAD 1009 Arch

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
Does anyone have an issue with cylinders in FactoryCAD objects not showing correctly (as lines) in an AutoCAD elevation view?

In AutoCAD Architectural 2009 when using the "BldgElevationLineGenerate" command to create a 2D elevation the cylinders contained in the FCAD objects do not show up correctly if the FCAD object being sectioned is within an xref. On the attached zip "drawing2" is a file that contains an FCAD conveyor and a section of that conveyor. The 2D section shows properly. In the file "drawing3", "drawing2" is attached as an xref and a 2D section is made of that xref. In this case the cylinders show up as lines.