Cancel
Showing results for 
Search instead for 
Did you mean: 

Envelopes on Factorycad control panels

Not applicable

Are future versions of Fcad going to have the option of creating an envelope above
& or below a control panel as needed? Many panels I use have connectors attaching
from underneath. Others have items on top or cables dropping in from above.
1 REPLY

Re: Envelopes on Factorycad control panels

Not applicable
Hello Mark,
At this time we do not have any plans to add safety envelopes above or below
the cabinets. I will add your request to the list for consideration in
future versions.
The only work around I can think of right now (and it is not real good one)
is to make the current envelopes taller than your cabinet for clearance
above and make the base taller for clearance below.
Thanks,
Brenda
"Mark Burns" wrote in message
news:424b0bac$1@bbsnotes.ugs.com...
>
> Are future versions of Fcad going to have the option of creating an

envelope above
> & or below a control panel as needed? Many panels I use have connectors

attaching
> from underneath. Others have items on top or cables dropping in from

above.