Cancel
Showing results for 
Search instead for 
Did you mean: 

Error wiht PS 10.1 after uninstall PS 11

Creator
Creator

Hi,

 

I have a big problem, I was using PS v11 only as a client. Then for working to another project I need to changed to PS v 10.1. So I have first uninstalled v11 and then installed v10.1 on my PC. I have only client installation. Now PS is completetly stuck, when i try to open the program a fatal error occured and PS crash. The error is realted to microsft error.

I try the procedure a couple of time with the same results. Did any one experience the same problem swithcing from v11 back to v10? 

 

2 REPLIES 2
Highlighted

Re: Error wiht PS 10.1 after uninstall PS 11

Valued Contributor
Valued Contributor

Hi

 

Please see attached fix to this issue. Bascially bad work was done on the .net version control between installations.

 

Regards

Re: Error wiht PS 10.1 after uninstall PS 11

Creator
Creator

Hi,

 

Unfortunatly I can't test it, I was not able to fix the issue so I keep going with V11.1. I talked with different people of technical assistance from Tecnomatix but no one was able to fix my problem.

 

 

So tahnk you very much! I really appreciate.

Ciao