Cancel
Showing results for 
Search instead for 
Did you mean: 

Export operations with hierarchy from process designer to excel

Experimenter
Experimenter

Hello,

 

I am trying to export operations with the tree hierarchy to excel. Is it possible or is there any special macro that can do that easier than writing it "manually"?

 

For example:

I want export structure on picture 0001 to excel so it will look like in the picture 0002 (there are two examples of exported table).

 

Thank you very much

 

Jesenius

 

1 REPLY

Re: Export operations with hierarchy from process designer to excel

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

 

the out of the box solution is to use Table View in Process Designer, define atributes (table colums) which should be exported and then export to excel.

The hierachy may be created directly in excel, I suppose.

 

Many customers have developed own solutions where exported data use templates so they get the data in proper form directly after the export.

 

Regards,

 

Martin