Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

FactoryCAD layer Control

N/A

After making the Layer Control to OFF status, i found that all the inserted FactoryCAD
objects are stil going to the same pre-designated layer and not to the current layer.
Is the problem in Release 11.0 only? I am currently using release11.0.
1 REPLY

Re: FactoryCAD layer Control

N/A

"gowri shankar" wrote:
>
>After making the Layer Control to OFF status, i found that all the inserted
>FactoryCAD
>objects are stil going to the same pre-designated layer and not to the current
>layer.
>
>Is the problem in Release 11.0 only? I am currently using release11.0.

Hi Gowri
I am not able to duplicate this in V11.0.
Please keep in mind that you need to shut down AutoCAD after you change the Layer
Control status for it take effect. If you do not shut down AutoCAD after changing
the Layer Control status, the objects will still be placed on the layers that they
are supposed to be on.
Regards
Deepak