Cancel
Showing results for 
Search instead for 
Did you mean: 

FactoryFLOW 13 reporting does not work

Not applicable
I'm confused with FactoryFlow reporting functionality. I'm trying to perform Reports -> Standard reports and every time I have the error message below:
The Visual Basic UFL that implements this function if missing (or U2lcom.dll is missing).
Error in file C:\TMP\blah-blah-blah.rpt.
Error in formula .
'crVolumePerTimeUnit({...blah-blah-blah...
This error occure when trying to build any type of standard report, though exact error messages differs (different functions cause this message). Seems to be not data specific (I've used the standard training data).
I use FactoryFLOW release 13 (with patches) with AutoCAD 2008 on WindowsXP, 32-bit architecture.
I have U2lcom.dll in C:\Program Files\Business Objects\2.7\bin (also tried to put it into C:\Windows\system32).
Do I need to install some additional software/libraries? I found no such requirements in documentation.
Vladimir
1 REPLY 1

Re: FactoryFLOW 13 reporting does not work

Not applicable

Hello Vladimir
We have not been able to duplicate this issue. However, one other user in Italy
(Radu Simionescu) was getting the same error. He was able to find a solution for
this problem and his suggestion was to add the following information the registry.
Thanks Radu :-).
***
Windows Registry Editor Version 5.00

@="CRUFLFlow.CRUFLFlow1"



@="mscoree.dll"
"ThreadingModel"="Both"
"Class"="CRUFLFlow.CRUFLFlow1"
"Assembly"="CRUFLFlow, Version=13.0.42.3, Culture=neutral, PublicKeyToken=4ac2168d6371d780"
"RuntimeVersion"="v2.0.50727"

"Class"="CRUFLFlow.CRUFLFlow1"
"Assembly"="CRUFLFlow, Version=13.0.42.3, Culture=neutral, PublicKeyToken=4ac2168d6371d780"
"RuntimeVersion"="v2.0.50727"

@="CRUFLFlow.CRUFLFlow1"
***
Copy the information above between the *** in notepad and then save the file with
a reg extension. Double click on the file and pick okay on the dialog when prompted
to enter the information in the registry.
You will have to restart AutoCAD and FactoryFLOW after this.
Regards
Deepak


"Vladimir Medvedev" wrote:
>
>
>I'm confused with FactoryFlow reporting functionality. I'm trying to =
>perform Reports -> Standard reports and every time I have the error =
>message below:
>
>The Visual Basic UFL that implements this function if missing (or =
>U2lcom.dll is missing).
>Error in file C:\TMP\blah-blah-blah.rpt.
>Error in formula .
>'crVolumePerTimeUnit({...blah-blah-blah...
>
>This error occure when trying to build any type of standard report, =
>though exact error messages differs (different functions cause this =
>message). Seems to be not data specific (I've used the standard training =
>data).
>
>I use FactoryFLOW release 13 (with patches) with AutoCAD 2008 on =
>WindowsXP, 32-bit architecture.
>I have U2lcom.dll in C:\Program Files\Business Objects\2.7\bin (also =
>tried to put it into C:\Windows\system32).
>Do I need to install some additional software/libraries? I found no such =
>requirements in documentation.
>
>Vladimir
>
>
>
><meta http-equiv="3DContent-Type" content="3D"text/html;" charset="3Dkoi8-r"" />
><meta content="3D"MSHTML" 6.00.2900.3627="" />
>
>
>
>

>
I'm =
>confused with=20
>FactoryFlow reporting functionality. I'm trying to perform Reports -> =
>
>Standard reports and every time I have the error message=20
>below:

>
 

>
The Visual Basic UFL that implements =
>this function=20
>if missing (or U2lcom.dll is missing).

>
Error in file=20
>C:\TMP\blah-blah-blah.rpt.

>
Error in formula =
>.

>
>size=3D2>'crVolumePerTimeUnit({...blah-blah-blah...

>
 

>
This =
>error occure=20
>when trying to build any type of standard report, though exact error =
>messages=20
>differs (different functions cause this message). Seems to be not data =
>specific=20
>(I've used the standard training data).

>
>size=3D2> 

>
I use =
>FactoryFLOW=20
>release 13 (with patches) with AutoCAD 2008 on WindowsXP, 32-bit=20
>architecture.

>
I have =
>U2lcom.dll in=20
>C:\Program Files\Business Objects\2.7\bin (also tried to put it into=20
>C:\Windows\system32).

>
Do I =
>need to install=20
>some additional software/libraries? I found no such requirements in=20
>documentation.

>
>size=3D2> 

>
>size=3D2>Vladimir

>
>