Cancel
Showing results for 
Search instead for 
Did you mean: 

File Client Cache is not enabled

Experimenter
Experimenter

If I start the Teamcenter Client , the following message is coming up:

 

File Client Cache is not enabled

 

FMS_HOME in my envrionment variables  is already set up.

 

Can someone help me . I don't know whats happen here?

 

My PC is using Win7

 

Thx!

8 REPLIES

Re: File Client Cache is not enabled

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you please tell us which application you are using Tecnomatix Plant Simulation, Tecnomatix Process Simulate, ...?

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: File Client Cache is not enabled

Experimenter
Experimenter

Hello, I'm speaking from Teamcenter 2007

 

Re: File Client Cache is not enabled

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello Try this:

 

open tc command promp:

This is in your start menu-> Teamcener (directory) -> command prompt with the version name

enter fccstat -status

 

If this return some numbers than it means that fcc is working fine and knows fsc details.

If this fails, then you need to see if FSC is working or started.

 

For windows: To check FSC: go the the server where you have installed FSC:

open services

Check the service with Teamcenter FSC ....

Make sure this is started.

 

if you find errors on fccstat -status : let me know the errors and we can troubleshoot.

please also respond with:

was it ever working?

did you applied patch?

change something?

installed new client? etc.

Re: File Client Cache is not enabled

Experimenter
Experimenter

Hello,

thank you for helping me!!!!!

But the issue is solved!!

The Problem was that the customer change some IP's and our company has to change

this in our Firwall. And now it is solved.!!

 

Kind regards

Stilo8

Re: File Client Cache is not enabled

Experimenter
Experimenter

Hi All,
when i am trying to launch Teamcenter getting below mentioned error....can any one please guide me to solve the issue

Re: File Client Cache is not enabled

Creator
Creator

it is not able to find the volume.

for work arround to login to teamcenter keep the line given below in portal.bat 

set TC_SKIP_CLIENT_CACHE=1

Re: File Client Cache is not enabled

Experimenter
Experimenter

Hello the issue is not slved

 

Re: File Client Cache is not enabled

Experimenter
Experimenter

Check database running and connected. This might be one of the reason.