Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Getting a MU attribute value

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

in this case you cannot use @

To set the value, an exit or entrance control would be the better approach.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Getting a MU attribute value

Creator
Creator

i am trying to get the value, not setting it. The value is placed already at the start of the model. There are 3 objects: V60, XC40 and V40. And the V60 has to go a slight different route. The attribute is already defined in the MU tabs on the library and doesn't change along the process.

Re: Getting a MU attribute value

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

if you only have three objects then you could create three global variables and store a link to the objects there (e.g. exit control of the source). Then you can access the parts everywhere in the model via the variable.

 

if you only have one instance of the MU, you can directly access the MU with e.g.

 

.MUs.V60:1

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net