Cancel
Showing results for 
Search instead for 
Did you mean: 

Import Logic Block --> Process Simulate

Experimenter
Experimenter

Hello !

 

Is it possible to create "Entries" and "Exits" with an other method ? Because it's very boring to click on "Add" --> "Bool", "Add" --> "Bool", "Add" --> "Bool", "Add" --> "Bool", "Add" --> "Bool",  ......

 

I need 2000 inputs and 2000 outputs.

1.jpg

So Please, if you have something a little more fun, tell me.

 

Sincerly

2 REPLIES 2

Re: Import Logic Block --> Process Simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

You could use the Tecnomatix.API to create your own function that allows you to create numbers of entries/exists.

 

OOTB that´s the only way to create LB entries/exits.

 

Best regards

Patrick

Re: Import Logic Block --> Process Simulate

Experimenter
Experimenter

OK , Thanks for your help again Smiley Wink