Cancel
Showing results for 
Search instead for 
Did you mean: 

In Kawasaki RCS mode, Robot can run Op successful in path editor, but stoped in sequence editor

Valued Contributor
Valued Contributor

11.PNG12.PNG

Hi All

 

I met a issue for robot simulation in PS software.

 

the path Op is running under Kawasaki RCS mode, it can be running very good in Path editor, but it is stoped in Sequence editor as attach snapshort.

 

If I closed the RCS mode, then it working both good under Path editor and sequence editor.

 

and each locations I have set the "Config",

 

can somebody give me direction on this issue ?

 

1 REPLY

Re: In Kawasaki RCS mode, Robot can run Op successful in path editor, but stoped in sequence editor

Valued Contributor
Valued Contributor

Issue is closed

 

since the program is imported from robot controller, need remove the OLP Sinals

 

then the robot running without failed

 

Thanks