Cancel
Showing results for 
Search instead for 
Did you mean: 

Layer Control - Object Status

Not applicable

How to set object status to have more options?
ex. GMs use status Protect for Plant Charter...
When using object status how XML can create the correct Layer instead of use CIMF_XML-N
(NEW) The correct must be object layer with "new" suffix.
ex. PR-ROBOT-BASE layer after set to new by using object status must be PR-ROBOT-BASE-NEW.
Thank you
Mechi
1 REPLY 1

Re: Layer Control - Object Status

Not applicable

"Rubens Mechi" wrote:
>
>How to set object status to have more options?
>ex. GMs use status Protect for Plant Charter...
>
>When using object status how XML can create the correct Layer instead of use
>CIMF_XML-N
>(NEW) The correct must be object layer with "new" suffix.
>ex. PR-ROBOT-BASE layer after set to new by using object status must be PR-ROBOT-BASE-NEW.
>
>Thank you
>
>Mechi
>

The robot xml object is placed on the cimf_xml layer by default and is then displayed
with properties of other layers. This is because "layer keys" have been set within
the object and also specific colors have been assigned to the robot segments.
Therefore, even though you may have moved the robot to some other layer, it may
not display the properties of the new layer.
If you want to assign the robot to a specific layer, then you may have to remove
all the "layer keys" that have been assigned to that robot.
If this is not clear (or if I have not answered your question), please contact GTAC
and we can setup a concall to discuss this further.
Regards
Deepak