Cancel
Showing results for 
Search instead for 
Did you mean: 

Object Enablers for Autocad 2010

Not applicable

Are there any FactoryCAD object enablers for Autocad 2010? We get FactoryCAD v11/Autocad
2007 files from supplier - and we have Autocad 2010. We only need to view/reference
the info, there is no need to change.
Thanks,
Andy Parrow
Deisgn Systems Inc.
5 REPLIES 5

Re: Object Enablers for Autocad 2010

Not applicable

Hello Andy
V14 of the Factory programs will be supported on AutoCAD 2010. The planned release
of v14 is in the Feb timeframe of next year. Therefore, at this time we do not have
any Factory enablers for AutoCAD 2010.
However, if you are just looking at viewing/referencing 2007/v11 files on your machine,
then you could request your supplier to send you an AutoCAD drawing with the Factory
objects saved with their proxy graphics. To save an AutoCAD drawing with the proxy
graphics you would have to do the following:
1. Select the "Save with Detailed Proxy Graphics" (F-Tools >> Export Utilities)
command.
2. Hit enter at the command line prompt to activate the routine.
3. You will see a prompt that says "Draw alternate proxy? :"
4. Enter "yes".
5. The command will return the following at the command line prompt "CIMF_DRAW_PROXY_MODE_BALLOONS_YES"

If you are in plan view and save the drawing, the drawing will be saved with 2d
information for the objects. If you save the drawing in an isometric view, then
the drawing will be saved with 3d information for the objects.
This setting is saved for the AutoCAD session only. If you restart AutoCAD, then
you will have to repeat the steps. This will also increase the size of the drawing
based on the amount of FactoryCAD geometry there is in the drawing and also on the
view (plan or isometric).
Hope this helps.
Regards
Deepak

"Andy Parrow" wrote:
>
>Are there any FactoryCAD object enablers for Autocad 2010? We get FactoryCAD
>v11/Autocad
>2007 files from supplier - and we have Autocad 2010. We only need to view/reference
>the info, there is no need to change.
>
>Thanks,
>Andy Parrow
>Deisgn Systems Inc.

Re: Object Enablers for Autocad 2010

Not applicable

Thanks for the quick reply. We have (1) seat of FactoryCAD v11 and 2007 here. So
we can do try for what we need to reference rather then going back to supplier.
Thanks again!
Andy
"Deepak Gokuldas" wrote:
>
>Hello Andy
>
>V14 of the Factory programs will be supported on AutoCAD 2010. The planned
>release
>of v14 is in the Feb timeframe of next year. Therefore, at this time we do
>not have
>any Factory enablers for AutoCAD 2010.
>
>However, if you are just looking at viewing/referencing 2007/v11 files on
>your machine,
>then you could request your supplier to send you an AutoCAD drawing with the
>Factory
>objects saved with their proxy graphics. To save an AutoCAD drawing with the
>proxy
>graphics you would have to do the following:
>
>1. Select the "Save with Detailed Proxy Graphics" (F-Tools >> Export Utilities)
>command.
>2. Hit enter at the command line prompt to activate the routine.
>3. You will see a prompt that says "Draw alternate proxy? :"
>
>4. Enter "yes".
>5. The command will return the following at the command line prompt "CIMF_DRAW_PROXY_MODE_BALLOONS_YES"
>
>
>If you are in plan view and save the drawing, the drawing will be saved with
>2d
>information for the objects. If you save the drawing in an isometric view,
>then
>the drawing will be saved with 3d information for the objects.
>
>This setting is saved for the AutoCAD session only. If you restart AutoCAD,
>then
>you will have to repeat the steps. This will also increase the size of the
>drawing
>based on the amount of FactoryCAD geometry there is in the drawing and also
>on the
>view (plan or isometric).
>
>Hope this helps.
>Regards
>Deepak
>
>
>"Andy Parrow" wrote:
>>
>>Are there any FactoryCAD object enablers for Autocad 2010? We get FactoryCAD
>>v11/Autocad
>>2007 files from supplier - and we have Autocad 2010. We only need to view/reference
>>the info, there is no need to change.
>>
>>Thanks,
>>Andy Parrow
>>Deisgn Systems Inc.

>

Re: Object Enablers for Autocad 2010

Experimenter
Experimenter
Any idea when FactoryCAD 14 is going to be released?

Re: Object Enablers for Autocad 2010

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
FactoryCAD V14 is scheduled to be released on April 30, 2010. This release will add support for AutoCAD and AutoCAD Architecture 2010, Windows 7, and Teamcenter 8.1.

Thanks
Kristy Myers

Re: Object Enablers for Autocad 2010

Experimenter
Experimenter
Thanks for the quick reply!