Cancel
Showing results for 
Search instead for 
Did you mean: 

PS: Operation Start Condition - Bug or Mistake?

Valued Contributor
Valued Contributor

Hello people, 

 

when trying to set an Operation Start Condition for any of my operations (Control -> Debug -> Operation Start Condition; I use it whilst having a simulation running), I always get the window that I am supposed to get, but I cannot type any text. It just doesn't react to my keyboard and no matter what I do (like copy, paste), it stays empty.

Is this a known bug (Process Simulate version 13.1.2) or am I missing something?

Thanks in advance.

3 REPLIES 3

Re: PS: Operation Start Condition - Bug or Mistake?

Creator
Creator

Did you solve it mate?

 

 

Re: PS: Operation Start Condition - Bug or Mistake?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

As you can see from the commands tooltip, it just a viewer no editor.

StartCond.png

 

To define your start condition for your operations you can use the "Transitions" in Sequence Editor.

Transitions.png

 

Best regards

Patrick

Re: PS: Operation Start Condition - Bug or Mistake?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi!

 

If I understand correctly, Transition is used to define conditions when next operation can start.

Operation Start Condition button is used to see conditions when operation actually starts. That is not the same, because operation can have two or more predecessors and each of them can have a transition condition. So Start condition is a calculated combination of two transitions and cannot be edited directly.

Regards, Vladimir.