Cancel
Showing results for 
Search instead for 
Did you mean: 

Pop-up window outside screen border (problem between 2 screens and 1 screen)

Experimenter
Experimenter

in the office I'm working with 2 displays, so the pop-up window are putted on the left screen, while the graphic viewer is positioned on the right screen.

 

The problem is when I'm working on undocked. I can see the graphic viewer, but the pop-up windows are still positioned on the left side, outside the screen border... 

De preferences of the PC-screen undocked are correct.

 

Is there a setting somewhere who can overrule the position?

or in total any help?

7 REPLIES

Re: Pop-up window outside screen border (problem between 2 screens and 1 screen)

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Can you please name the product you are using? It will help us to answer your question properly.

Re: Pop-up window outside screen border (problem between 2 screens and 1 screen)

Experimenter
Experimenter

Hi,

 

I'm working with Process Simulate version 10.1, 38

 

PC is Dell M6700, OS Win7, SP1, 64-Bit.

 

Is this enough?

Re: Pop-up window outside screen border (problem between 2 screens and 1 screen)

Siemens Phenom Siemens Phenom
Siemens Phenom

Probably nVidia tools (nView Display Manager) provide some settings on this issue.

 

Also you can use a universal workaround. When dialog is opened outside the visible desktop, press:

Alt-Space, ENTER, Left arrow.

And then move the mouse Smiley Wink

Regards, Vladimir.

Re: Pop-up window outside screen border (problem between 2 screens and 1 screen)

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

If you would like to reset your menus location you need to open Tecnomatix Doctor and in the Tools menu select Reset Dialog Position

 

Thanks,

Avi

Re: Pop-up window outside screen border (problem between 2 screens and 1 screen)

Experimenter
Experimenter

Hi,

 

I am having the same problem with RobotExpert (V11,44).

 

I Reset Dialog Position with RobotExpert Doctor, but the pop-up window is still somewhere outside borders.

 

Do you have any idea?

 

Thanks,

Pedro Raposo

Re: Pop-up window outside screen border (problem between 2 screens and 1 screen)

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

What I usually use in such cases, is the layout manager. Try to switch to a predefined layout.

 

D.

Re: Pop-up window outside screen border (problem between 2 screens and 1 screen)

Experimenter
Experimenter

Change this setting in Windows 7:

 

Control Panel - Display - Change Display Settings - Multiple Displays - Show Desktop only on 1.

 

 

Similar options for other operating systems need to be set.

 

regards,

kiran