cancel
Showing results for 
Search instead for 
Did you mean: 

Process Designer Refresh Bug

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Forum,

 

We are having an issue with Process Designers (V10) GUI not updating when changes are made in any of the trees. e.g. Checking in/out, renaming, moving files etc.

 

The tree can be updated by clicking the "Show'Hide Columns" button but then you have to browse all the way back to where you were working within the structure wich is quite annoying.

 

Apparently this is a common issue that has been around for a while (multiple GTAC cases) but no solution has been found that I know of.

 

We've even been playing around with the solutions of the "Windows 7 Refresh Bug"  but with no avail.

 

Has anyone else experienced this before?

Is there another workaround/solution?

 

Cheers,

Hermias

3 REPLIES

Re: Process Designer Refresh Bug

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
Please run a REFRESH SCHEMA and ANALYZE SCHEMA from the Admin Console on the server.



This task should be completed weekly.



Michael Mood
Digital Manufacturing CoE

Siemens PLM Software II Inc.

Tel. (734) 953-3827
Cel. (248) 470-0865

Re: Process Designer Refresh Bug

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks for the feedback Mike!

I'll do that ASAP and get back regarding the results. Seems that this would do the trick.

Re: Process Designer Refresh Bug

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Seemed that it was a database issue with Tables in Oracle running out of space, which we could only see when we tried to refresh the schema. (We have 10 users in a training environment)

Thanks to you we could pin-point it.