Cancel
Showing results for 
Search instead for 
Did you mean: 

Process Simulate: Sensors in EquipmentPrototypes

Valued Contributor
Valued Contributor

Hello people,

I am quite new in Tecnomatix and have a question that is probably a bit stupid, but I just can't find a solution to it: I have an ordinary EquipmentPrototype in a ResourceLibrary. Loading this into my study is never a problem, until I add Sensors (Photoelectric Sensor or Property Sensor) into the structure of the EquipmentPrototype. I just drag&drop the EquipmentPrototype into the 3D view of my (in standard mode) loaded study.Unbenannt.png
I'm using version 13.1.2. Any ideas what I'm doing wrong?


Thanks a lot for your help

1 REPLY

Re: Process Simulate: Sensors in EquipmentPrototypes

Valued Contributor
Valued Contributor

Maybe I should be more specific: 
The light sensor is assigned to a 3D-file and can be displayed and added to the object tree by itself and once added to a study, I can assign it to an EquipmentPrototype, the only problem is when I try to load this prototype from a library into another study. 

Please help, sensors are quite important for my work and I don't want to manually readjust them everytime.