Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Process Simulate customizations

Creator
Creator

Hallo all!
A faced a problem . I have to install Process Simulate11.1  with a lot of controllers (fanuc,ABB,kuka krc & vkrc, and maybe some more) on more than 10 PC's. I already found the way to automate the installation using the .bat-file and looks like it works fine. But ...
Now I need to setup all the PC's the same way , with custom columns, custom keyboard shortcuts, and maybe custom menus.
So the question is - where all these values and settings are stored? As long as I found, the column data is in file PedColumnDataAll.xml at C:\ProgramData\Tecnomatix\Process Simulate\11.1. Maybe there is another way to share those custom columns , but it's all I found so far.
Is there a better way to copy all the customizations across the pc's? Keyboard shortcuts, menus...

1 REPLY 1

Re: Process Simulate customizations

Siemens Phenom Siemens Phenom
Siemens Phenom

I think these settins are user-dependent and at least some of them are stored in user profile:

%USERPROFILE%\AppData\Local\Tecnomatix\Process Simulate\<version>

 

Maybe it's possible to customize one worstation first and then copy configuration to others.

 

Regards, Vladimir.