Cancel
Showing results for 
Search instead for 
Did you mean: 

Revolute movement in Process Simulate

Pioneer
Pioneer

I have a resource that is supposed to make a revolute movement controlled by a PLC. The PLC has to know the current location of the resource in degrees and has to return a value where it has to move to, also in degrees. Is it possible to achieve this in Process Simulate, and if yes; how?

3 REPLIES 3

Re: Revolute movement in Process Simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Yes you can do this.

Therefore, you need to add a LB to your resource/device.

Inside the LB you can create a parameter "Joint Distance Sensor". It´s return value is e.g. "REAL".

This parameter you have to transfer via LB exit to any signal which is communicating with your PLC.

2018-05-09 09_56_50-Resource Logic Behavior Editor - Device.png

 

Best regards

Patrick

Re: Revolute movement in Process Simulate

Pioneer
Pioneer

Hi Patrick,

 

Thanks for your reply.

How do I connect this parameter to the LB exit? I created the parameter and an exit signal in the LB, but not sure how to connect these two.

 

Thanks in advance!

 

Re: Revolute movement in Process Simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

When creating a LB exit of type "REAL", just put "jds_parameter1" in value expression of the exit.

Just start typing "jds_" and it will show you the list of proposals.

At least, you should have a signals of type REAL. Add it in the area of the exist under "connected signals".

 

Best regards

Patrick