Cancel
Showing results for 
Search instead for 
Did you mean: 

Robcad covert to Process Designer failed (Cannot run "Export To eMS" command)

Experimenter
Experimenter

Hello:

 

Now I need convert some Robcad cell to Process Designer. And I'm already update EMS library and upgrade .co files.

 

But running robcad connectivity studies is failed. 

image.pngimage.png

image.png

The error report said:

Node Id: 352142 Description:
Tune Connection:
ERROR: Cannot run "Export To eMS" command.

 

I had tried several different .ce cells, even a nearly empty station also failed. And the error is same.

The picture below is the cell files need convert. My Process Designer version is 13.1

image.png

 

Thank you for your help!

 

1 REPLY 1

Re: Robcad covert to Process Designer failed (Cannot run "Export To eMS" command)

Creator
Creator

 

 

Hi,

 

You need to set up .ce file in Robcad though eMserver integration. for that you need seperate license.

 

 

a.png