Cancel
Showing results for 
Search instead for 
Did you mean: 

Run Time Error Problem

Experimenter
Experimenter

Dear all,

 

I just downloaded Technomatix 13 student version, but I'm unable to run the program due to the following error, has anyone experienced the same earlier, pls help me out. Thank you.

 

Technomatix error.JPGRun time error

1 REPLY 1

Betreff: Run Time Error Problem

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Shivaraj,

 

I've never seen this problem. Please check if there is a newer version of the graphics driver available.

 

If you're working with Windows 7 you could also try to change the Windows theme either to Aero or to a non Aero theme.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.