Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulation of Automated fiber placement using Process simulate 12

Experimenter
Experimenter

Hello everyone,

Part of my final thesis is to simulate a basic "automated fiber placement" cell using process simulate 12 in my university. I'm new to the software and facing difficulties in the simulation of fiber placement part. I know there are 3rd party applications such as vericut for these kind of tasks but my project requires me to perform it in process simulate itself.

 

Can anyone help or suggest a solution for me to display the tapes or fibers along the movement of robot head. Any contribution would be quite helpful in my task completion.

Thank you very much in advance.

 

Regards,

Ram Krishna.

2 REPLIES 2

Re: Simulation of Automated fiber placement using Process simulate 12

Siemens Phenom Siemens Phenom
Siemens Phenom

I think there's no good way to do it.

However you can try to use paint functionality. This module can color surface parts which were touched by paint fan.

 

PS: Whoops, sorry... paint functionality appeared in 13.0. That won't work for version 12.

Regards, Vladimir.

Re: Simulation of Automated fiber placement using Process simulate 12

Experimenter
Experimenter
Thank you for the reply Vladimir.
That was a helpful solution, however as you said me working on Process Simulate 12 is still a problem for me to accomplish the result.
Thanks for the help anyway.
Cheers Smiley Happy