Cancel
Showing results for 
Search instead for 
Did you mean: 

Solidwork 3D model to Tecnomatix plant simulation, Is it possible?

Experimenter
Experimenter

Hi all,

 

Im struggling to import my 3d model from solidwork to tecnomatix plant.

I even read all tutorial from siemens but there are no detail explaination for importing 3D model from 3rd party software.

 

I really glad if you can help me as soon as possible.

 

Best Regards

2 REPLIES 2

Re: Solidwork 3D model to Tecnomatix plant simulation, Is it possible?

Siemens Phenom Siemens Phenom
Siemens Phenom

Tecnomatix Plant Simulation supports to import JT files and VRML files.

 

The JT file format is an ISO standard for 3D data exchange. But I don't know if SolidWorks can write this format. In any way it should support to write VRML files.

 

If information is lost in the VRML export and you have access to our product Teamcenter Visualization you can use this application to convert other standard formats like IGES, STEP and STL to the JT format.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
Highlighted

Re: Solidwork 3D model to Tecnomatix plant simulation, Is it possible?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

you need to get the JT Translators for Solid Works. This will allow for the models to be exported from Solid Works then imported into Plant Simulation.