Cancel
Showing results for 
Search instead for 
Did you mean: 

TcMX v13.1a Missing Feature???

Experimenter
Experimenter

In our previous TcMX version (v12.1, if I remember correctly) I had a *very* usefull feature that allowed me to group entities, name these groups and through them, control object visibility (NOT related to the "Logical Collections Tree"). It was a small window with my group names and the light bulbs (on/off). Don't remember the command name. I'm not able to find this feature in the new version 13.1 (with MS ribbon style interface).

 

Where can I find this tool???

 

Thanks in advance!!!

 

5 REPLIES

Re: TcMX v13.1a Missing Feature???

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Do you mean "Display by Type"?

 

This dialog you will find in the "Graphic Viewer Toolbar"

displaybytype.png

 

Best regards

Patrick

Re: TcMX v13.1a Missing Feature???

Experimenter
Experimenter

Hi, Patrick.

 

No. Not that one. In the one I'am refering to I had the ability to create and name groups from selected parts on the screen.

 

Thanks!!!

Re: TcMX v13.1a Missing Feature???

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

You said it´s not the "group" command which is related to "Logical Collection Tree".

There are other commands like,

- Group to compound

- Create Device Group

 

 

But if these are not the functions I have no more idea which dialog or function you are looing for.

 

 

 

Re: TcMX v13.1a Missing Feature???

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

I think I found the function you are looking for.

 

You need "Save Selection" to save the corrently selected objects.

And you need "Retrieve Selection" to Display/Blank the created selections.

 

You have to customize the two commands into your Ribbon bar because by the default they are not customized.

 

Best regards

Patrick 

Re: TcMX v13.1a Missing Feature???

Experimenter
Experimenter

 

EXACTLY!!!!!!

That's what I was looking for.

 

Thank you so much.