Cancel
Showing results for 
Search instead for 
Did you mean: 

Technomatix Client Builder 7.5 hangs in upper left hand corner of screen

Experimenter
Experimenter

Hi,

 

When we start Client Builder 7.5 it minimizes to a small window in the upper left corner of the screen. At this point we can't maximimize the window or do anything else other then close the window. Previously the program worked fine so we are not sure of the cause. The computer in question is on a closed network(no internet access).

 

Does anyone have any suggestions? Is a reinstall necessary to fix this.?

 

See attached photos.

Mike

 

 

20161018_083131.jpg20161018_084819.jpg