Cancel
Showing results for 
Search instead for 
Did you mean: 

Triangular Distribution

Pioneer
Pioneer

Hello,

 

Is there a way to set upper and lower bounds within a triangluar distribution?

 

So if a=0, b=35, c=4 is there a way to ensure the samples are only taken between 2 and 30?

1 REPLY

Re: Triangular Distribution

Siemens Phenom Siemens Phenom
Siemens Phenom

No, since the last two arguments are already the lower and upper bounds.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.