Cancel
Showing results for 
Search instead for 
Did you mean: 

Two different PSZ with different libraries on emserver

Creator
Creator
Hello,

I had two different studies on emserver. For some reason I took PSZ of each study and started working on it. I modified libraries of these two studies. Product data is also changed and updated on psz.

Now again if I want to update my studies on emserver how shall I do it?

3 REPLIES 3

Re: Two different PSZ with different libraries on emserver

Siemens Phenom Siemens Phenom
Siemens Phenom

Please check Process Simulate online help:

 

emsupdate.JPG

You will have to update each separate library back to the sysroot first. Hopefully, none of the changed items are shared between the 2 PSZ's, then you need to decide which shall be the primary item.

Highlighted

Re: Two different PSZ with different libraries on emserver

Creator
Creator
Thank you Ray for the information.

I have one more query. I am getting emserver update failed issue with one of the study.other studies are updating properly.

Please check if you can help me out with attached image.

Thanks

Re: Two different PSZ with different libraries on emserver

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi.

You would need to check the eMS.log for a specific error, but that appears like you are trying to update some object in the Project where your user does not have some specific permission granted in the Amin Console/User Administration for that type of data.

Ray