Showing results for 
Search instead for 
Did you mean: 

UniCAM FX centroid importer has wrong x,y coordinates


I'm trying to import a centroid file into UniCAM FX, and the resulting x,y values are way off. The numbers in the file range in the 1000's (eg: x2002, y3001), but in the job editor the x,y values are showing up like 234,0435.12345, 354,654.34567645. Huge numbers with long decimals places. There is nothing like that in my file. Also, the views end up reducing the view to 1% scale. I have no idea why this is happening.