Cancel
Showing results for 
Search instead for 
Did you mean: 

Unknown command "FCONFIG" error after loading factory customization files in Autocad

After loading all the necessary customization files for FactoryCad 2016 in Autocad 2016 getting following errors,

--- Unknown command "FCONFIG" (while checking "Factory Configuration")

--- CIMFCAD; error: no function definition: CIMF_USECADLICENSE (while loading FactoryCad icon)

 

PFA snaphots for reference.

 

 

Please help me resolve this issue, because of which am not able to work with FactoryCad.

2 REPLIES

Re: Unknown command "FCONFIG" error after loading factory customization files in Autocad

Siemens Creator Siemens Creator
Siemens Creator
  1. To load the menus try using the FACTORY command rather than loading the cuix manually. This loads the menus but also sets trusted paths for the application.
  2. If this does not work run CimfCleanRegistry17.exe (default location is C:\Program Files\Siemens PLM Software\Factory Programs XXXX\Program) and try the FACTORY command again. Additional information can be found in the Factory Install Guide.  

Re: Unknown command "FCONFIG" error after loading factory customization files in Autocad

Experimenter
Experimenter

Thanks a lot! Your post resolved my problem loading FactoryFLOW.