Cancel
Showing results for 
Search instead for 
Did you mean: 

Weibull Distribution

Pioneer
Pioneer

In the help function it states the code used for weibull is z_weibull(stream, alpha, beta). If I wish to apply the following weibull information how would I use the above distribution function?

 

Location = 78

Shape = 0.6161

Scale = 32500

Minimum = 78

Maximum = 448000

1 REPLY

Re: Weibull Distribution

Siemens Phenom Siemens Phenom
Siemens Phenom

alpha is the shape parameter and beta is the scale parameter. It's not clear what location should specify so I'd suggest the following call:

z_weibull(1,0.6161, 32500, 78, 448000)

The first parameter here is the random stream. You can choose a different number to get another independant random stream.

 

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.