Cancel
Showing results for 
Search instead for 
Did you mean: 

Worker is present on SingleProc, but works just 25%

Pioneer
Pioneer

Hello,

 

do you have any cool idea on how to solve a problem:

 

I have a SingleProc where the part comes and worker must be present. But Worker is just watching the process, but in 25% of the cases he must interup and do the work.

 

Can you help me on how to do that.

 

regards

2 REPLIES

Betreff: Worker is present on SingleProc, but works just 25%

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello HugoZupan,

 

you can define a service called 'watching' for the SingleProc and also define a service 'watching' for the worker. At the singleproc also define an availability of 75% and a service 'working' which is also defined at the same worker. Later on you can examine the different services using the workerChart object.

 

Hope this will help.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Worker is present on SingleProc, but works just 25%

Pioneer
Pioneer

GG, thank you so much