Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

can i use the Container to model the pallet?

Experimenter
Experimenter

Hi all,

 

I am very new to this Plant Simualtion thing. Please help me.

 

How to model putting the parts from the Buffer onto a pallet? 

 

can i use the Container to model the pallet? For example, i set the Buffer to hold 200 parts before being put on a pallet.

 

after that, how to model moving the pallet to the production store? do i use the Transporter to model a worker pushing the pallet [Container] on the Track?

 

thank you

2 REPLIES 2

Re: can i use the Container to model the pallet?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Shahir,

of course, that is possible.

I prepared two examples with the Tansferstation or with programming.

The model is for Plant Simulation 12.0

Regards,

Peter

Re: can i use the Container to model the pallet?

Experimenter
Experimenter
Many thanks Peter for your help. I really appreciate it.

I couldn't find the TransferStation in the Class Library. I believe that it should be under the Material Flow?

Please help.

Many thanks in advance.