Cancel
Showing results for 
Search instead for 
Did you mean: 

create a batch from one Source with differen MUs and batch sizes

Pioneer
Pioneer

 

Dear team,

 

for my master-thesis I need to set up a production side. Therefore I have one Source which should create different MUs with different Batch sizes and different production times of each batch in the Single Proc.

The batch size of each MU should be the size which is listed in the table "Komponente". The production time of each batch in the Maschine should be as listed in Table "BZ3". These batches should be produced in one batch and beginning from the Single Proc "DMC" it should be dismanteled to one pieces.

 

I tried the VDA var Source already or also to match a Carrier with MUs before moving into the Single Proc. without success.

 

Thank you for your help.

 

Unbenannt.png

1 REPLY 1

Re: create a batch from one Source with differen MUs and batch sizes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
please post it again in the Plant Simulation forum
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net