Cancel
Showing results for 
Search instead for 
Did you mean: 

path import in PS

Experimenter
Experimenter

Hello,

Like robcad, is there any provision in PS for loading path in Emserver???

I will explain more clearly...If 2 person work on some project, one on Emserver and one one standalone, how the paths made in standalone mode will import to Emserver.

4 REPLIES 4

Re: path import in PS

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

You can download your path from Standalone enviornment and upload into your eMServer environment.

 

or

 

If the study you are working in Standalone is coming from the eMS Study, you can update eMS from PSZ.

If user A is working on operations for Robot 1 in Standalone and User B is working on operation for Robot 2 you will not have any problems when updating from PSZ.

If you both work on the same the operations on eMS will be update with the operations from Standalone.

 

Best regards

Re: path import in PS

Experimenter
Experimenter

Sorry, can you more specific about first option.

Re: path import in PS

Experimenter
Experimenter

Thank you for your responce...

Re: path import in PS

Siemens Phenom Siemens Phenom
Siemens Phenom

About the first option.

 

Just select the operation you created in PS Standalone, in Operation Tree, right mouse click -> download.
Afterwards you will have your operation downloaded to file system in your robot vendor syntax.

This you can upload into PS on eMS. Therefore open Program Inventory for your selected robot and upload the operation.

 

Best regards

Patrick