Cancel
Showing results for 
Search instead for 
Did you mean: 

put two part one next the other on one line

Pioneer
Pioneer

Hi

I want to know if it is possible to put 2 MU . one next to the other on the same line  .it must look like this.Capture1.PNG

 

Please help me 

Thanks

2 REPLIES 2

Re: put two part one next the other on one line

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Manu,

as long as MU1 and MU2 move together the two MUs could located on a container.

Please note that it is bettter to sent such question to the Plant Simulation Forum.

Regards,

Peter

Re: put two part one next the other on one line

Pioneer
Pioneer

Hi,

Ok thank for this information