Showing results for 
Search instead for 
Do you mean 
Reply

use the perl to create instance , at the last step,i enter the wrong password?

2016-07-22_121709.png

anyone knows the instance whether create successfully ?and what ican do to resolve the problem but reinstall the ORACLE or instance ?

 

 

2 REPLIES

Re: use the perl to create instance , at the last step,i enter the wrong password?

Best thing you can do is deleting Oracle instance.

Please try to use Oracle 11.2.0.4 which officially tested and compatible with the perl script. 

Re: use the perl to create instance , at the last step,i enter the wrong password?

yes,the best way !if you don't  recreate the instance,it can't connect to oracle, eventhough the listener is 

working 。oracle12g,the last password is used to create the listener correctly !