Cancel
Showing results for 
Search instead for 
Did you mean: 

worker

Creator
Creator

Hello All,

Help me please with my problem. I want to model it in such a way that one worker is operating on 4 stations. I have marked 'Active' on 'Importer', and then in 'Services' I have named this service 'Metax'. I did it in all 4 stations, but if I start model, worker is working only on station1 and station2 - station3 and station4 are unsupported.

Is the error due to the buffer being in the middle?

Also I have done an exit strategy for this process. Or maybe I shouldn't do it?

I want worker to work on station1 then station2, station3, station4

And I want the process to proceed in order station1-station2-buffer-station3-station4

Thanks in advance!

 

1 REPLY 1

Re: worker

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

there is a Plant Simulation forum, it is better if you post your questions there

 

can you post your model? I guess there are some settings wrong.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net