Cancel
Showing results for 
Search instead for 
Did you mean: 

xt2jt conversion

Experimenter
Experimenter

Can  we also convert the 3D graphics formats to JT files using the program xt2jt that is installed in the Plant Simulation installation folder?

Here, 3D graphics I mean the point cloud files imported from the 3D scanners.

Anyone please elaborate the usage of installing xt2jt, if possible send me few sample files.

 

Regards

Shubha

1 REPLY

Re: xt2jt conversion

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Shubha,

 

xt2jt cannot convert point cloud files to jt.

 

You can use xt2jt on the command line as follows:

    xt2jt.exe <InputFile> -output <output JT file> -monolithicJT

 

The following formats are supported:

Parasolid Text Files (*.x_t; *.xmt_txt)
Parasolid Binary Files (*.x_b; *.xmt_bin)
PLMXML Files (*.plmxml)
CATIA V4 Files (*.exp; *.model)
IGES Files (*.iges; *.igs)
STEP Files (*.step; *.stp)

 

Regards,

Ralf