Cancel
Showing results for 
Search instead for 
Did you mean: 

JT 4 Office - Imported Views

Pioneer
Pioneer

In my source file  (generated in NX9)  i have several section views. 

 

This source file is translated to JT and the sectional views are correct in JT2GO (11.4.0).

 

When i load the 'HTML' file into JT 4 Office (word 2016) the 'Model Views' are available for selection. The sectional views show the full geometry, not the sectioned geometry which i see in JT2GO which means the 'Snapshot' is incorrect.

 

Am i doing something wrong?

 

Thanks in advance,

 

R.

5 REPLIES 5

Betreff: JT 4 Office - Imported Views

Legend
Legend

Hello @rosswoodward,

Sorry sections are not possible to view at the moment in HTML generated with JT2Go.

 

best regards

Wolfgang

Betreff: JT 4 Office - Imported Views

Pioneer
Pioneer

Thank you for the response.

 

The workaround i have employed is to manually create a screen-shot (via windows 7 - snip) and replace the snapshot bitmap in the word doc.

 

Cheers,

 

R.

Betreff: JT 4 Office - Imported Views

Legend
Legend

@rosswoodward

Yes this can be a solution.

Printing is possible also from JTGo.

If you have as example a pdf printer you can use this also for generating pictures (jpg, bmp, png...)

Than you have better results for presentations.

Betreff: JT 4 Office - Imported Views

Siemens Phenom Siemens Phenom
Siemens Phenom

The version of the viewing solution in the JT 4 Office add-in did not support section views at the time that it was published.  I have talked with the team responsible for the data generated for the html page and the viewer and it sounds as if the problem has been resolved in a more recent version of the end to end solution.  I will bring this up with Product Management to determine how to proceed with this.

Betreff: JT 4 Office - Imported Views

Pioneer
Pioneer

Cheers Rick,

 

Thats good to know.

 

R.