Cancel
Showing results for 
Search instead for 
Did you mean: 

I can not open Examples in JT Open Toolkit

Experimenter
Experimenter

Hi Experts!

Recently, i have  downloaded the JT open Toolkit. I installed it according to the Siemens Guidance and then Firstly i tried to follow the Get_Started_Doc in the Program and wanted to open the Geom_Simple Example. After i did so and also gave my Sold_To_ID, i tried to run the app, but i got some weird Errors as below :

 

'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Program Files (x86)\Siemens\JTOpenToolkit\8_5\example\Geom_simple\geometry_VS2013_Win32_Debug.exe'. Symbols loaded.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\ntdll.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\kernel32.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Unloaded 'C:\Windows\SysWOW64\kernel32.dll'
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\kernel32.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\KernelBase.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\apphelp.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\msvcp140d.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\vcruntime140d.dll'. Cannot find or open the PDB file.
'geometry_VS2013_Win32_Debug.exe' (Win32): Loaded 'C:\Windows\SysWOW64\ucrtbased.dll'. Cannot find or open the PDB file.
The thread 0xa14 has exited with code -1073741701 (0xc000007b).
The thread 0x4ed4 has exited with code -1073741701 (0xc000007b).
The thread 0x47f8 has exited with code -1073741701 (0xc000007b).
The program '[20356] geometry_VS2013_Win32_Debug.exe' has exited with code -1073741701 (0xc000007b).
 
I have already read the software prerequisite (e.g. Visual Studio 2015) and install them too, what would be the Problem and how can i solve it?
 
my final intention is to open .JT file and just see that and may transform it.
 
I would be grateful of any help and answer.
 
1 REPLY 1

Re: I can not open Examples in JT Open Toolkit

Siemens Legend Siemens Legend
Siemens Legend

If the sample project file is compiling successfully and you have an executable you probably have some issues in the environment. Take the .exe file and drop it in the lib directory for your platform and see if it runs from there.

Mike Z