Cancel
Showing results for 
Search instead for 
Did you mean: 

JT_PMI_CONTENT_HINT automatically generated on save?

When read a JT file using JT Open Toolkit, then save the loaded data using JtkCADExporter::exportJt, and then read the resulting JT file again using the Toolkit, I see some new properties which were not there when saving the file, for example, JT_PMI_CONTENT_HINT. Interestingly, JT2Go doesn’t see this property. Is this property automatically generated by the Toolkit on saving? How can I disable this automatic generation of properties?

3 REPLIES 3

Re: JT_PMI_CONTENT_HINT automatically generated on save?

Siemens Legend Siemens Legend
Siemens Legend

Hi,

As you noted this is a hidden property, it can be used to know when a file has PMI content. It is not controlled through a JT Open Toolkit API call though.

Mike Z

Re: JT_PMI_CONTENT_HINT automatically generated on save?

So this property is always added and there is no way to disable it?

Re: JT_PMI_CONTENT_HINT automatically generated on save?

Siemens Legend Siemens Legend
Siemens Legend

Correct, there is not a way to turn it off in the JTTK.

Mike Z