Cancel
Showing results for 
Search instead for 
Did you mean: 

JT to HTML for websites / Android / iOS

Experimenter
Experimenter

Dear All,

 

My company is developing websites, mobile apps for automotive aftermarket.

 

My client is ready to share JT files for 3D viewing of each part on our site / solutions. But there are some limitations. Actually with JT file, user must be installed with JT2GO viewer & file will get download on his system & then only he can see the file using this viewer.

 

My query is how they can generate HTML output from PLM (teamcenter), so that I user need not require any separate viewer as well as no need to download the each JT file. 

1 REPLY 1

Betreff: JT to HTML for websites / Android / iOS

Legend
Legend

Hello @Aftermarket

it is already possible with JT2Go 11 as desktop version or as WIn 10 App to generate HTML files.

For more it is to use here PLMvis.

Also a good option can be the Solid Edge Portal or Sky DRM (cooperation with JT2Go and Siemens).

An example how the output can be looking I place under here.

 

Best Regards

Wolfgang

Test_Picture_HTML_JT2Go.PNG