Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

JTOptimiser - How to set the output Unit

Creator
Creator

Hi,

 

I am using JTOptimizer to reduce the file size. But when I import the file into NX once again after conversion units are changed to Meters instead of mm. Due to this model is scaled to 1000 times. Can you please help me to resolve this issue.

 

Regards,

 

Thadeus.D

1 REPLY 1

Re: JTOptimiser - How to set the output Unit

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

it does not work with JtOptimize.exe. You can use Jtattributte.exe it is part of "JtUtilities" to add ModelUnit to your JT and set the Value =mm

 

jtattribute.exe  -a  <type> <key> <value>   Adds an attribute.

 

 

Drago